Grey background

Terminal Venting

Provides information to heating, air conditioning and refrigeration service technicians about an important safety issue: terminal venting.

Terminal Venting

What is terminal venting?

If a compressor’s electrical terminal pin is damaged, weakened or otherwise loses its seal and separates from the compressor terminal, pressurized oil, refrigerant and debris may spray out. This is called “terminal venting.”

The ejected debris, oil, and refrigerant can injure people or damage property. The oil and refrigerant spray can be ignited by electrical arcing at the terminal or any nearby ignition source, producing flames that may project a significant distance from the compressor. The distance depends on the pressure and the amount of refrigerant and oil mixture in the system. The flames can cause serious or fatal burns and ignite nearby materials.  

A variety of abnormal conditions can cause terminal venting, including internal or external electrical faults/shorts, or mechanical damage to the terminal or compressor.

Read More...
Click to continue reading What is terminal venting?
How do I know if terminal venting is about to occur?
What precautions should I follow during servicing to reduce the risk from terminal venting?
How can I reduce the risks of terminal venting when energizing the unit after service?
If a compressor does not use flammable refrigerants, is there still a risk of fire or explosion?
Read More...
Click to continue reading
Please enable JavaScript to use this website.