Emerson Introduces Copeland™ Variable Speed Reciprocating Hermetic Compressors for Refrigeration

Designed to deliver energy efficiency and performance improvements for commercial refrigeration applications to meet impending energy and refrigerant regulations

Emerson Introduces Copeland™ Variable Speed Reciprocating Hermetic Compressors for Refrigeration

Copeland™ variable speed reciprocating hermetic compressors for commercial refrigeration applications

ST. LOUIS, March 3, 2021 – Emerson (NYSE: EMR) announced the introduction of its Copeland™ variable speed reciprocating hermetic compressors for commercial refrigeration applications. The new models are specifically engineered to save energy and provide performance improvements in a variety of demanding commercial refrigeration applications.

Original equipment manufacturers (OEMs) in the commercial refrigeration space have faced increasingly stringent energy requirements. Medium- and low-temperature stand-alone coolers and freezers, commonly used in restaurants, convenience stores (C-stores) and small-format food retailers, have been key targets of the Department of Energy’s (DOE) energy-efficiency standards. Additionally, targeted are units used in the life science market and for small industrial applications such as process chillers. The DOE will also soon be proposing its next phase-down in energy reductions for these applications, likely to take effect in 2024. This means that OEMs are seeking a competitive edge by offering equipment that helps them achieve ENERGY STAR® certification and delivers the energy-efficiency levels that will allow refrigeration units to meet upcoming DOE requirements.

Copeland variable speed reciprocating hermetic compressors for refrigeration are comprised of two components:

  • Copeland variable speed reciprocating hermetic compressor, available in ranges from 1/8 to 7/8 horsepower, which features a brushless permanent magnet motor, versus a standard induction motor.
  • Copeland variable speed drive which has a smart controller integrated within it.

“The wide availability of operating ranges, combined with the breadth of the low-profile Copeland variable speed reciprocating hermetic compressor line, gives system design engineers options to select compressors that deliver optimum energy efficiency for equipment of varying types and sizes,” said Derek Langenkamp, hermetic reciprocating product manager for Emerson’s cold chain business.

Variable speed capabilities with smart controls can help deliver significant energy and performance improvements that far exceed fixed capacity options. While assisting customers in the redesign of their systems at Emerson’s test labs, they have increased system energy efficiency by 13 percent, reduced compressor cycling by 90 percent and lowered compression ratios by 43 percent compared to a high efficiency fixed speed system using propane (R-290). This means faster pulldowns to setpoint temperatures, more precise temperature holding, less wear and tear on system components and lower energy bills.

By utilizing the natural refrigerant R-290 with a low global warming potential (GWP) of 3, OEMs can offer their customers a more sustainable refrigeration option that meets some of the most stringent refrigerant and energy-efficiency regulations, including the potential impending 2024 DOE standard, California Air Resources Board standards and potential Environmental Protection Agency refrigeration requirements.

For more information on Copeland variable speed reciprocating hermetic compressors for refrigeration, please visit our website. And for more information on Emerson refrigeration, cold chain and air conditioning technologies, visit copeland.com.

About Emerson

Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial and residential markets. Our Automation Solutions business helps process, hybrid and discrete manufacturers maximize production and protect personnel and the environment while optimizing their energy and operating costs. Our Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information, visit Emerson.com.

For more information, contact:
Michelle Crawley
[email protected] / 937-890-5311

Please enable JavaScript to use this website.