C037-global_temp-817023732

Estimates have suggested that the use of HFCs alone could cause a 0.5-degree rise in global temperatures.

Ahead of the curve, and the competition.

At Copeland, we don’t believe in “one refrigerant fits all.” A comprehensive portfolio of products and solutions designed for a variety of refrigerants enables our customers to find the right fit for their architecture and create efficient, F-Gas-compliant, future-proof systems. Ultimately, these tailored solutions optimize system performance, decreasing lifecycle costs and becoming more environmentally friendly and sustainable in the process.

Read More...
Click to continue reading Ahead of the curve, and the competition.
Woman shopping along the chiller aisle

Where do we go now?


There is no single perfect refrigerant for the diversity of air conditioning, refrigeration, and industrial applications. The predominant halocarbons (CFCs, HCFCs, and HFCs) combine excellent efficiency and safety with acceptable costs. But they contribute to ozone depletion potential (ODP) and global warming potential (GWP).

 

In response to the catastrophic damage caused by these halocarbons, the Montreal Protocol mandated the phase-out of CFCs and HCFCs in 1987. Despite positive ozone layer recovery, alternative HFCs have since been shown to still cause climate change, with a GWP significantly greater than CO2. Estimates have suggested that HFCs alone could cause a 0.5-degree rise in global temperatures.


Sustainability challenge accepted.


As the phasedown of HFCs continues globally, the challenge is to identify truly sustainable alternatives that maximize environmental, economic, and operational benefits. Next-generation refrigerants with low global warming potential (LGWP) include natural options like carbon dioxide (CO2), hydrocarbons (HC), and ammonia (NH3), as well as HFO and HFO blends. Environmental policy must take into consideration the pros and cons of all options. ​​​​​​​

Please enable JavaScript to use this website.